AXIS#.BODE.EXCITEGAP

Description

AXIS#.BODE.EXCITEGAP controls how often the excitation is updated. The excitation is updated every n drive samples, where n is AXIS#.BODE.EXCITEGAP. For example, if AXIS#.BODE.EXCITEGAP = 2, then the excitation is updated every 2/(16,000 Hz) = 1/8,000 Hz = 0.000125 sec. When measuring a system, update the excitation only as often as the data is recorded.

Example

Set excitation update rate to 8,000 Hz:

-->AXIS1.BODE.EXCITEGAP 2

Set excitation update rate to 4,000 Hz:

-->AXIS1.BODE.EXCITEGAP 4

Get excitation update rate (already set to 8000 Hz):

-->AXIS1.BODE.EXCITEGAP 2

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

Drive samples

Range

1 to 255 drive samples

Default Value

2 drive samples

Data Type

Integer

Stored in Non Volatile Memory

Yes

Variants Supported

All variants are supported

Related Topics

Using the Performance Servo Tuner | Using the Performance Servo Tuner: Advanced

Scope

Axis Settings

Parameter and Command Error Messages

 


Stay Connected with Kollmorgen

Copyright © 2018 Kollmorgen